What is a magnetostrictive level sensor used for?
These level sensors are used as measured value pick-ups for the continuous recording of levels, and are based on determining the position of a magnetic float according to the magnetostrictive principle.
How does a level sensor work?
These level sensors work on the float principle with magnetic transmission. The float's magnetic system actuates a resistance measuring chain that corresponds to a 3-wire potentiometer circuit in the guide tube.