What are diaphragm seals?
Diaphragm seals, also known as remote seals or chemical seals, basically have two tasks. Firstly, they separate the measuring device from the medium and secondly, they transfer the pressure to the measuring device and can be disassembled very easily and quickly for cleaning and calibration purposes.
When should you use diaphragm seals?
They are typically used in application areas where the process medium should not come into contact with the pressurised parts of the measuring instrument. This protects the measuring instrument and extends its service life.
In which sectors are sanitary diaphragm seals mainly used?
Sanitary diaphragm seals are used primarily in industries that require a high level of sanitation. For example, in the pharmaceutical and beverage industries as well as in the water purification industry. Sanitation-conscious manufacturers gain a high level of safety and efficiency by using WIKA measuring instruments that are equipped with sanitary diaphragm seals.To achieve the required degree of purity in these areas, high temperatures and various chemicals are used in sterile or sanitary facilities. A diaphragm seal is therefore required in this environment to protect the measuring device and helps to extend its service life.
What is the WIKA Build ID?
The WIKA Build ID is a unique seven-digit code that temporarily saves an individual WIKA instrument configuration. The WIKA configuration can be saved, shared and used later using the Build ID.
How long is the WIKA Build ID valid?
The WIKA Build ID is valid for at least three months.