- Industries
- Industrial
- Heating, ventilation and air-conditioning technology
- Heat transfer and distribution stations
Heat transfer and distribution stations
District heating – one module in the efficient use of resources. Using energy through combined heat and power (CHP) and at the same time greatly boosting the efficiency rating of the system – one of the outstanding advantages of local and district heating.
The principle of combined heat and power (CHP) is to take waste heat that would otherwise be unused, e.g. from electricity-generating power plants, and to supply it to consumers, even over long distances, thereby increasing the utilisation level of these power plants to as much as 90 %.
To assure problem-free connection to the district and local heating network, the operators devise their own technical connection requirements (TAB). These stipulate how and under what conditions a house station can be connected to the supply network, either directly or indirectly. Depending on the measurement task involved, you decide which of our mechanical, mechatronic or electrical measuring instruments to use. There is a choice of different output signals, switching functions and measuring elements, meaning that you have no problem integrating these in any plant concept for open-loop or closed-loop control purposes.