WIKA

Submersible pressure sensors

For every hydrostatic level measurement, the right submersible pressure sensor

The submersible pressure transmitter, sometimes also referred to as a level probe, is a specific design of pressure sensor for hydrostatic level measurement in tanks, wells, shafts and bore holes. For this, the submersible pressure transmitter is submerged directly in the liquid to be measured, and positioned as close as possible to the bottom. There, the submersible pressure sensor measures the hydrostatic pressure, which enables a direct conclusion regarding the current level, i.e. the height of the liquid column above it.
FAQ
FAQ

What is the overpressure limit?

Pressures up to the overpressure limit will not cause any permanent damage to the measuring instrument, however, the error limits specified in the data sheet could be exceeded.

Where is the submersible pressure sensor installed?

The submersible pressure sensor is installed at the lowest measuring point.